We need to drive a single-turn coil for a calibration-loop antenna, with a diameter of approximately 50cm, and at frequencies of the order of 100Hz to 10kHz. We need to have a very high output impedance (at least tens of kOhm), so that the calibration coil does not disturb the surrounding magnetic field, and a current output of approximately +/-20mA.
Is the OPA615 suitable for this application? It is listed as a DC restoration circuit, which has nothing to do with our application, but the output impedance and current capability appears to be suitable.
Is the OPA860 better suited for this application? It has a reasonable output impedance and current.
Is there any other amplifier that would be better?
Thank you for your help. Ben