Other Parts Discussed in Thread: TLE2064BM, TLE2064, OPA4192, LM2901, LM139, OPA1622, OPA4172
Looking for any assistance in confirming the output current capability of the TLE2064BM operational amplifier.
Per the absolute maximum ratings it says the output capability is +/-80mA and that total current into Vcc+ is +80mA and current out of Vcc- is -80mA.
Since this specification is provided under absolute maximum ratings section I believe the +/- 80mA applies to the whole device and not per amplifier but want to make verify.
It is also unclear if the +/-80mA allotment can be divided up between the four amplifiers as necessary or is there a maximum per amplifier?
Thanks