Other Parts Discussed in Thread: INA219
Hi!
Is it also possible to detect the current direction with the INA219?
I want to use it for monitoring charge/discharge of a battery.
I saw in the datasheet that there is a difference between the V_SHUNT input voltage of the 219 and 226. The 219 says "max: +/-40 mV" and the 226 "min: -81.9175 mV, max: 81.92 mV"
I assumed that the output of the 219 would be always positive but this is what I wanted to know.
Thanks!
David