Other Parts Discussed in Thread: PGA309
Hello, Kay. I'm Daekeon.
I wrote that 3-points(-10, 25, 80 degrees) calibration data didn't save EEPROM properly.
I attach the Cal-Result file and saved calibration data file to EEPROM. The whole calibrations are sucessful so Cal-Result is proper.
As you know when seeing the EEPROM data file, It didn't save properly. Why was this problem happened?
Also, i wonder if my calibration Model file and Pre-Cal file are right. Please check them.(refer to attached files)
Finally, I want to know my DMM Scripts files contained Iout file and Vout file are proper.
In DMM Scripts, Are the pause and num of stopbits values very important? When i changed them, Calibration couldn't work it.
Can you recommend the DMM Scripts setting to calibrate ??
Again, Thank you very much for your cooperation^^
TPS30_Vout_MN_0_SN_1057to1072_DT_5115.xls
[EEPROM Data] Addr0 = 21577 Addr2 = 0 Addr4 = 0 Addr6 = 1408 Addr8 = 1050 Addr10 = 0 Addr12 = 5172 Addr14 = 36328 Addr16 = 0 Addr18 = 33788 Addr20 = 34188 Addr22 = 32767 Addr24 = 0 Addr26 = 30328 Addr28 = 65535 Addr30 = 65535 Addr32 = 65535 Addr34 = 65535 Addr36 = 65535 Addr38 = 65535 Addr40 = 65535 Addr42 = 65535 Addr44 = 65535 Addr46 = 65535 Addr48 = 65535 Addr50 = 65535 Addr52 = 65535 Addr54 = 65535 Addr56 = 65535 Addr58 = 65535 Addr60 = 65535 Addr62 = 65535 Addr64 = 65535 Addr66 = 65535 Addr68 = 65535 Addr70 = 65535 Addr72 = 65535 Addr74 = 65535 Addr76 = 65535 Addr78 = 65535 Addr80 = 65535 Addr82 = 65535 Addr84 = 65535 Addr86 = 65535 Addr88 = 65535 Addr90 = 65535 Addr92 = 65535 Addr94 = 65535 Addr96 = 65535 Addr98 = 65535 Addr100 = 65535 Addr102 = 65535 Addr104 = 65535 Addr106 = 65535 Addr108 = 65535 Addr110 = 65535 Addr112 = 65535 Addr114 = 65535 Addr116 = 65535 Addr118 = 65535 Addr120 = 65535 Addr122 = 65535
[Filenames] Pre-Cal Filename = "TPS30_Iout_-10,25,80_Vref.txt" DMM Script Filename = "Current_34401_rs232.txt" [Misc] Comments = "" Serial No = 1176 Model No = 0 Model ID = "TPS30_Iout" Mux Size = 16 Error Tolerance = 0.300000 Samples to Average = 2.000000
[Filenames] Pre-Cal Filename = "TPS30_Vout_-10,25,80_Vref.txt" DMM Script Filename = "Voltage_34401_rs232.txt" [Misc] Comments = "" Serial No = 1193 Model No = 1 Model ID = "TPS30_Vout" Mux Size = 16 Error Tolerance = 0.300000 Samples to Average = 2.000000
[PGA309_Settings] Numb Reg = 3 Poly Order = 1 Output Mode = 2 Vout_High_Target = 3.949440 Vout_Module_High_Target = 5.000000 Vout_Module_Low_Target = 1.000000 Iout_High_Target = 0.020000 Iout_Low_Target = 0.004000 Vout_Low_Target = 0.429440 Vs = 5.000000 Vref = 4.096000 Calibrate Nonlin = TRUE Calibrate Coarse Offset = TRUE Reg0 = 0 Reg1 = 0 Reg2 = 0 Reg3 = 1280 Reg4 = 0 Reg5 = 0 Reg6 = 5172 Reg7 = 0 Reg8 = 0 Temp0 = -10.000000 Temp1 = 25.000000 Temp2 = 80.000000 XTR_R1 = 11000.000000 XTR_R2 = 11000.000000 XTR_R_ref = 200000.000000 XTR_Vref = 4.096000 Secondary Output Stage = FALSE Second Stage Gain = 1.000000 Second Stage Offset = 0.000000
[PGA309_Settings] Numb Reg = 3 Poly Order = 1 Output Mode = 0 Vout_High_Target = 5.000000 Vout_Module_High_Target = 5.000000 Vout_Module_Low_Target = 1.000000 Iout_High_Target = 0.000000 Iout_Low_Target = 0.000000 Vout_Low_Target = 1.000000 Vs = 5.000000 Vref = 4.096000 Calibrate Nonlin = TRUE Calibrate Coarse Offset = TRUE Reg0 = 0 Reg1 = 0 Reg2 = 0 Reg3 = 1280 Reg4 = 0 Reg5 = 0 Reg6 = 5172 Reg7 = 0 Reg8 = 0 Temp0 = -10.000000 Temp1 = 25.000000 Temp2 = 80.000000 Secondary Output Stage = FALSE Second Stage Gain = 1.000000 Second Stage Offset = 0.000000