Other Parts Discussed in Thread: BUF634
Hello,
I'm planning on using the buf634 as current buffer inside an opamp loop as described in the datasheet in figure 24.
In my application the buffer will be connected to +/-15v supply with +/-11.8v 400hz input
The output current can reach 220mA
According to the datasheet the output voltage swing decreases with temperature and output current so I thought on paralleling two buffers.
I know there is issues with connecting opapms in parallel as described in:
e2e.ti.com/.../paralleling-op-amps-is-it-possible
But is there problem with paralleling buffers inside unity gain opamp loop?
I have attached my pspice circuit which worked fine in the simulation.