Other Parts Discussed in Thread: PGA202
A PGA202 at 60db has 37mVrms of output noise with less than 1uVrms at the input. This is with 47pF added to the compensation pins for 100KHz bandwidth.
The same measurement is 50mVrms with no capacitors added [1MHz bandwith].
Still with 100KHz bandwidth, changing the gain to 40dB, 20dB, and 0dB results in noise voltages of 3.7mVrms, 260uVrms, and 10uVrms respectively.
Given the input noise voltages and noise voltage densities in the data sheet, are these measurements the levels I should expect, or is there something I should resolve?
Thank you for you help, Dave.