Other Parts Discussed in Thread: ISO122, ISO124
Are there any differences between the ISO122 and ISO124 other than nonlinearity gain? The book price for the ISO124 is lower even though the nonlinearity gain is better so I'm trying to understand if there is anything else I'm missing.
Also, how does the signal propagate through if the power supplies are different on each side? Is there a gain or could the signal simply hit the rail?
For my design +/-15V is available at the input so that’s easy, but only 0 to 9V at the output. I don’t understand how its referenced. Let’s say I have a 1Vpeak sine signal riding on 2.5VDC on the input, so it goes between 1.5 and 3.5V. When that gets output from the ISO124 with the 0 to 9V supply, does it try to match the center of the supply rails (treating it as a +/-4.5V supply) and can preserve this signal? Or maybe it sees the input signal as centered 17.5V above the negative supply such that the whole signal is clipped? I just want to understand what to expect at the output.