This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA552

Good morning,

I used OPA552on my card with the following characteristics:

Vcc  9 to 25Vdc

Gain x10, non-inverting

Vin 0.5Vdc with Vout 5Vdc or Vin 1.25Vdc with Vout 12.5V or Vin 2Vdc with Vout 20Vdc 

Iout 200mA

The VCC changes along with the selection of the VIN.

I had no problems but rechecking the data sheet I understand the minimum Vin = V- + 2.5V .

If so should be the input is not polarized is then VOUT wrong .

What I did not understand?

Davide Gandolfi