This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA282 Start-up Transient Response



Hello,

Can you please explain why do we get this type of transient response please ?Page 10 of the datasheet, figure 20.

If Vin+ = 0V, will the transient response be different ?

Thanks! Mohamed

  • Hello Mohamed,

    The figure quoted shows output versus supply voltage, under the condition of a fixed differential input of 50mV. The transients are due to a combination of (1) low supply condition and (2) the switched capacitor architecture (SC) of the input stage of the amplifier. When supply is low (<2.7V), not every component of the internal circuit is fully functioning. In addition, the SC circuit takes at least a clock cycle to accurately sample the input voltage. Once the input is correctly sampled then the output slews to final value of 2.5V

    By “Vin+=0V” do you mean the differential input equals 0V? If so I would not expect this kind of transient, the output should be around 0V(limited by SWING)

    Regards,

    Guang-Apps Current Sensing Products