Other Parts Discussed in Thread: LM7121, LMH6723, OPA890, THS4221, THS4222, SN10501
Dear community,
I struggle to find the right amplifier for my application, mainly because it requires a high voltage (>11V) and a perfect 0V (negative supply needed).
The main specs are :
- Unity gain stable
- Slew rate > 500 V/us
- Alim positive > 12 V
- Alim negative < -1 V
- Swing min. +11.5V
If the symmetrical supply is necessary, the LM7121 is almost good, but not enough.
If we can use a -1V / 12V supply, the OPA890 or the LMH6723 are much better and much cheaper.
The footprint also depends on this strategy.
Is there any specific amplifier which can handle -1V / +12V supplies ?
Thanks in advance.