Other Parts Discussed in Thread: OPA350, PCM4202, OPA1632, LM833
When i use the OPA350 in non inverting configuration with Rg = 2k7 and Rf = 1M
when i feed 5mV to the positive Input via Frequency Generator i Need to set an
DC Offset of 2,5mV to get a full swing Output. Without Offset i only get the upper
half wave. Is that normal ? What to do to avoid this ?
Kind regards
Michael