Other Parts Discussed in Thread: INA2331, INA331
Hi,
I am using an INA2331 as a differential amplifier for a single varying resistor bridge. I am using it with single supply of 3.3V, therefore, I have an external reference of about 1.65V. The expected output of the bridge is up to 14mV, and the gain used is of 110 using R2=21k, R1=1k, and the shutdown pin is connected to V+
The circuit I am using is as the one depicted in Figure2 of the datasheet.
However, with an input of 4mV, the output I measure at the output is even below the reference, and therefore get a negative value.
Is there more calculations needed to set a correct reference voltage? My input is DC so I am not sure how to apply the input common mode calculations in the datasheet. Can someone see what I am doing wrong?