Other Parts Discussed in Thread: LM7705, OPA350
I am looking for a suitable active low pass filter (second order) to convert a differential input to a unipolar output.
Input: Each input channel is varies between 0-5V. The net input voltage V1-V2 varies between -2.5 to +2.5V
Output: 0 to 3.3V
The output has to be fed to an ADC that accepts unipolar or positive voltages only. Please suggest something.