I am using LM13700 transconductance op-amp to generate a sawtooth waveform by connecting a capacitor at the buffer output. Firstly, it is very difficult to improve the linearity of this IC. I tried to use the linearizing diodes by giving them +15V bias ( and a series resistor of 15k to limit the diode current). I am only able to achieve linearity till 60 mV. I want to achieve a better linearity say 10 mV to 100 mV atleast. Please suggest me some ways to improve the linearity of this IC.
Also, in the datasheet it has been mentioned that the IC has 2MHz bandwidth. However, I am not able to achieve the sawtooth frequency over 500 kHz. There is no gain vs frequency curve given in the datasheet so it is really difficult to determine whether this IC is suitable for this high frequency range.