Hi,
I'm designing a voltage-to-current converter (e.g. based on Figure 13 in the INA114 datasheet), trying to achieve 100pA accuracy, so I need an op-amp with low offset voltage and input bias current. I have a couple questions about the LMP2011:
*On page 7, the datasheet lists the Input current as -3pA, and the Input offset current as 6pA, but Figure 6 on page 9 shows an Input bias current of ~125 pA at a 2.5V common mode voltage. Is there an inconsistency here? Or is this reporting the AC value (as explained in section 7.4.1), while the earlier chart lists the DC value?
*Section 7.4.1 says that at high temperatures, the input currents become much larger, with 0.5nA typical. Does a chart exist for input current vs. temperature? I don't think I see one on the datasheet, and my application is very sensitive to this variable.
Thanks,
Jake Bernstein
Synthetic Neurobiology Group
MIT Media Lab