Other Parts Discussed in Thread: OPA1622, TIPD177
Is there additional care to be taken while obtaining balanced output from OPA1622 (using two op-amps)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Chethan,
A major consideration in balanced output (bridge-tied loads) is stability because the amplifier output effectively sees half the load impedance (e.g. double the capacitance). It's important to do a full stability analysis of each amplifier by breaking the feedback loop and checking the phase margin with an equivalent load impedance. As Tim mentioned, in TIPD177 I showed a network which mimics the high frequency behavior of a headphone (assuming this is a balanced headphone amplifier application) but a 400 pF capacitor is also a simple way to represent the impedance of headphones at high frequency.