Other Parts Discussed in Thread: INA300, INA301
Hey. I drive a dc motor. It's nominal voltage 6v and no load nominal current is 22mA. I want to know the current of the motor therefore i might know the torque of the motor. For example if the current is above the 100mA i'll stop the motor. For that, i need a current sensing device. One directional current..I connect the sensor to the microcontroller. So i don't need ADC i think..don't i? Thanks in advance.