What is the maximum differential input voltage that the LMH6553 can safely handle and then recover from?
I have an experiment where I drive a line with pulses of 500 MHz RF at around 10 Vpp. I then need to amplify small transient voltages on that same line (echoes, akin to pulsed NMR) and feed that to an ADC.
I currently use switches in front of my amplifier which i turn off while driving the line with 10 Vpp so as not to saturate the amplifier. However, if LMH6553 could handle 10s of volts on its input, clamp the output to say 2 V, and then recover in 600 ps, this would be much simpler.
Thoughts?