Other Parts Discussed in Thread: INA121, OPA192
Hello,
I'm working on a project where I have to design an amplifier and a filter for a sensor. The sensor is a hydrophone and this generates a differential voltage proportional to movement in water. It has a piezo electric element inside. The output of this sensor usually is around the 10 mV so I decided to have an amplifier with a gain of 100 V/V (40dB) to obtain an output of approximately 1V.
My question is, will a I need an amplifier with differential voltage inputs? Let's say for example like the instrumentation amplifier INA121. Or will the design of a single input non-inverting amplifier work?
I ask because I'm a little confused with the connections. Also, the output of the hydrophone is a BNC cable so I would have to connect a BNC Female connector to the amplifier, right?
**The hydrophone output goes to the amplifier. The filter is already designed and is working**
Many questions so thanks in advance for taking your time :)