- Is the common mode range of a current sense amplifier relative to the chips ground?
- The voltage across a 100mV shunt in a bidirectional application will be -100mV to +100mV
- In a low side application one side of the shunt will be connected to ground so the shunt voltage will be ±100mV relative to ground
- The common mode range of many of your current sense amplifiers which say they are low side and bidirectional capable only extends to 0V
- Therefore using the shunt as described above would cause the amplifier inputs to go outside the specified common mode range
What am I missing?