This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Low side bidirectional current sensing

  1. Is the common mode range of a current sense amplifier relative to the chips ground?
  2. The voltage across a 100mV shunt in a bidirectional application will be -100mV to +100mV
  3. In a low side application one side of the shunt will be connected to ground so the shunt voltage will be ±100mV relative to ground
  4. The common mode range of many of your current sense amplifiers which say they are low side and bidirectional capable only extends to 0V
  5. Therefore using the shunt as described above would cause the amplifier inputs to go outside the specified common mode range

What am I missing?