Other Parts Discussed in Thread: XTR111-2EVM, XTR111
Hello,
I am trying to use the XTR111-2EVM as a current source to power the specimen. A sinusoidal wave oscillated at 100Hz~2000Hz will be the input signal. The peak-to-peak amplitude ranges from 0.5V~1.5V. I am wondering whether the XTR111-2EVM is able to deal with the negative portion of the input sinusoidal signal and what the linear output range of the XTR111-2EVM is.
Thanks in advance.
Best,
Lei