Other Parts Discussed in Thread: LM7171
Hi,
I am using LM7171 in non inverting amplifier configuration. Tina schematic of the circuit is below:
The results in TINA show output as pulses varying between 13.65V and -13.65V with rise time of some 39nsec giving slew rate of about 558V/us.
Here are the actual results that have same component values with same supply range.
Here, it is seen that LM7171 is taking 1.4us to swing between -13.2 and 13.6 V, hence giving slew rate of about 14V/us.
Why is this considerable difference is there. Also, when datasheet says 4100V/us, why in TINA even it gives 558V/us.
Look forward for reply.