Other Parts Discussed in Thread: LM8272, LM8261, TINA-TI
A capacitive load of 800 nF (a piezo actuator) has to be driven with a step function. For example: first step 5V and 4 following steps of 1.0 V each. Slew rate 1 V/ms.
After reaching the maximum voltage (10V), the 'capacitor' needs to be discharged within 10 ms (Vin = 0V),
but that may be done by an additional comparator and FET if not possible by the OpAmp.
From the maximum output current, an OPA209 or OPA192 may be suited for a resistive load, but I expect not for a capacitive load.
Any recommendation which OpamAmp may be better suitable? There will be a +12V single supply. Required output 0 to 10V The OpAmp will be driven from a 12 bit DAC, preferably with internal reference like a TLV5636. In this case the OpAmp is in a non-inverting configuration with a gain of around 2.5


The upper curcuit is like the one we have discussed showing the results predicted by you.