Other Parts Discussed in Thread: OPA170, LM321, OPA237
Hi All,
I have a circuit that will limits current and I set to 150mA maximum based on my design, I need to charge a huge capacitor 8mF with this 150mA, I need 5A current with a duty cycle of 4% on R1(R1 is an active load that consume 5A in span of 200uS with a period of 5mS), This 28V will dip once the switch is ON with 200uS(as normal), This is my application that I want to add this current limit circuit.
When I simulate this circuit I can limit the current to 150mA which is good but once I prototype it Headache arises, I always use OPA170 Opamp for my prototype but I cannot get any success on this this OPAMP which always got damage, Once I increase the current more than 150mA, Is there any problem with my OPAMP selection? If so can you recommend any OPAMP that is suitable with my application. Or is there any problem with the circuit. I found the circuit on this site
electronics.stackexchange.com/.../active-current-limiter
I am hoping some help from expert/s.
Thanks and regards,
Jay