This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Triangular Wave Generator for a fixed frequency

Hello,

I'm trying to build a triangular wave generator for a fixed frequency of 10 kHz. I'm trying to create a simple circuit. I've seen some simple examples that uses a multivibrator that generates a square waves and then is pass through a integrator to generate the triangular wave. I also seen VCO that generates triangular waves, but all the circuits I've tried to simulate just doesn't work. It is a little frustrating.

To be more specific, I need a triangular wave generator that goes from 0V to 5V with a fixed frequency of 10kHz. That's basically all. 

Any help or tip will be appreciated.

Thanks!