Other Parts Discussed in Thread: INA217
Hello !
I'm trying to use the INA217 or current sense amplification. I was happy to find this part because of it's high bandwidth at 40dB gain, which is what I am looking for.
However, I noticed that feeding 70kHz sine wave to the amplifier (5Ohm sense) already outputs a significant phase shift (a few percent). As it is meant for phase analysis of electrochemical systems, I cannot allow the amplifier to have such a phase shift. Weirdly, the same shift also appears for another INA on the board with 6dB gain only.
I checked the input of the INA (by referencing the other input to GND) and the signal is in phase with the input, and I checked at the output, and the signal is slightly out of phase with the input
Is this something I should have expected from this part ?