Other Parts Discussed in Thread: OPA4172, OPA4171, OPA171, TLV2374
I use the quadruple OpAmp OPA4172 in a new circuit. One of the 4 opamps is used as a comparator:
Pin 2: 100k to GND, 460k to Vin (voltage to be compared)
Pin3: 10k to stable 2.5V-reference, 330k to pin 1 (hystereses).
Supply-voltage: 12VDC
The comparator works correctly and has the following measured (and calculated) thresholds of Vin: Output pin1 goes low for Vin >15.6V and output goes high for Vin< 13.6V.
However, if the input Vin is 0V (or not connected), I measure 1.1V at the pin2. This corresponds to a current of roughly 10uA out of pin 2, but bias-currents are specified with some pA in the OPA4172-datasheet.
My questions:
What is the reason for this high voltage on pin2?
Why is the current out of pin2 higher than the bias-current specified in the datasheet?
Is the differential voltage pin2 to pin 3 too high for this opamp (I did not find a limiting specification for this in the datasheet)?
Will the OPA4171 work correctly used as comparator, as described above? We do not need speed, but accuracy.
Thank you in advance for your advice!