Other Parts Discussed in Thread: LM6171, LMC6082
Hi,
I'm trying to design the first stage (transimpedance amplifier) of a radation detector with a "common" photodiode.
Sytem details:
The goal of the first stage is to have a pulse when some kind of radiation impact the photodiode. This will produce a 15/20 nA - 50 us pulse.
Photodiode: Vishay BPW34 (70 pF - 2 nA dark current in photovoltaic mode (0V bias))
Necessary bandwidth: 20 kHz.
The transimpedance amplifier seems to be ok with low frecuencies. I've simulated a 3 photodiode array with C1 (capacitance = 210 pF), IS1 (dark current = 6 nA) and IG1 (a 15 nA - 50 us pulse).
Naturally, the capacitance of the photodiode begins to cause problems with frequency. As is indicated in most technical literature, the photodiode can be bootstrap with a voltage follower, improving the bandwidth. But when I've tried it I begin to have problems.
This is, for example, the AC gain with a LM6171 as voltage follower:
What I'm doing wrong?
Thanks!Transimpedancia 01.TSC