Other Parts Discussed in Thread: XTR117, TL431
i am using XTR117 IC for my project .There is a Vreg on pin 8 and Iret on pin 3. can i use this both pin to power my microcontroller with 5 V ????
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, this is exactly what the VREG output is meant for. I strongly suggest you take a look at the following blogs which describe how to avoid many common pitfalls when designing 2-wire 4-20mA transmitters:
2-Wire 4-20mA Sensor Transmitters: Background + Compliance Voltage
https://e2e.ti.com/blogs_/b/precisionhub/archive/2014/11/04/two-wire-4-20-ma-transmitters-background-and-common-issues
2-Wire 4-20mA – IRET Can’t connect to Vloop GND
https://e2e.ti.com/blogs_/b/precisionhub/archive/2014/12/09/part-2-two-wire-4-20-ma-transmitters-background-and-common-issues
2-Wire 4-20mA – IRET < 4mA
https://e2e.ti.com/blogs_/b/precisionhub/archive/2015/01/13/two-wire-4-20ma-transmitters-background-and-common-issues-part-3
2-Wire 4-20mA – Controlling 2-Wire Transmitters with Externally Powered Sources
https://e2e.ti.com/blogs_/b/precisionhub/archive/2015/02/24/two-wire-4-20ma-transmitters-background-and-common-issues-part-4
2-Wire 4-20mA – Input Isolated Sensor Transmitter

Hi Chirag,
The MPS430 devices are low power, but they are most +3.3V devices which means you would need a +5V to +3.3V LDO to power the MSP430. This could be achieved with a simple device like the TL431, or an integrated LDO IC.
I suggest you post a question on the low-power DC/DC converters forum for assistance selecting a product for this application.
thanks Collin Wells.
i want one more help from you.
can you suggest me if i want to go in cypress than which is best MCU in cypress for this application???
hi Collin Wells,
i have decided i will make this application in MSP430.
Now can you suggest me which MSP430 device i have to use for this particular application??