Other Parts Discussed in Thread: INA282
We are using the INA282AIDR current sensor in an application where we measure current draw from a 30V battery on the high side.
We have been using the sensor in our design for about 1 year and it has been functioning as expected. We have currently had a number of cases where the circuit has drawn excessive power and triggered shut down procedures.
The current measuring circuit functions such that the power to the INA282 is turned on and off to conserve power. The datasheets specify that the INA282 can be used in this format.
The failure rate we are getting is about 5%. We have traced the source of the excess power to the INA282 through the sense pins. We traced the lot codes of the INA282 that are failing to
- AQDJ G4 - 15 failures
- C16P G4 - 7 failures
Where the previous lot in our production 'AQDK G4' functioned fine.
We are not sure if our design is such that we are on the edge for how we are using the INA282, or if something has changed in the manufacturing process of the INA282.
Please respond with any questions as we need to resume production.
Below is the circuit.