Other Parts Discussed in Thread: LMH7324
i have a pulse digitalization application
pulses are 10ns - 100ns with a repetetion rate of 20uS and current from photo diode is arround 500uA - 70mA so the drop accross 50ohm sense resistor would be 2.5mV - 3.5V, i want to use LMH7324 for this purpose to directly digitalize the pulse, with out using any further amplification, what are the implications of doing so ??
if above is not wrong how to generate a stable reference voltage of 1mV ?