Other Parts Discussed in Thread: BUF634, THS3091, LM7171
I am looking to amplify the current of a 3.3v, 50% duty cycle, 40MHz square wave from the output of my function generator. I need this signal to drive a 50 ohm load with a drive current requirement of approximately 65mA. The output impedance of the function generator is 50 ohm and the output square wave signal is being fed through a 50 ohm BNC cable. I am thinking about using an Op-amp and Buffer combination to amplify the square wave signal from the function generator in order to provide the required drive current. I want to use the BUF634 high speed buffer device in a closed loop with an op-amp to achieve my requirements. I would think a gain of 2 or 3 would be sufficient.
I am somewhat unclear about how to design this circuit. Could a suitable op-amp be suggested to compliment the BUF634 device (Needs to be capable of driving high speed signals e.g. 40MHz) ? I also want to know what supply voltages are required to be supplied to both the V+ and V- rails of the BUF634 and the op-amp for my requirement. It would really help to have a schematic to visualize what type of circuit I am dealing with.