Other Parts Discussed in Thread: LMV324S, LMV324, LMV344
Hi
I am using a handful of LMV324s in a low frequency fixture. Supply voltage is +5V. Problem is on every instance of this on PCB, but we can discuss just one instance. U6-B, a unity gain buffer, sees a 0V (within a couple millivolts, best I can tell) to 900mV pulse, 20% duty cycle, 1/2Hz. Very pedestrian signal, right? The rise and fall time is about 1ms. The output swings from 42mV to 900mV, then back down to about 48mV, then a 300ms decay back to about 42mV.
I have verified the chip is indeed grounded. All other aspects of the amplifier seem valid, but it just does not seem to like to swing to ground. I have added 1k pull down resistors with no effect.
Your thoughts?LED Controller Board SCH -JRG May 25.pdf