Other Parts Discussed in Thread: INA326, TIPD170, INA333, INA331, INA321
Dear Forum
I have a water level sensor which changes its resistance from 400 ohm to 1500 ohm depending on the water level. It also includes a temperature dependent resistor used to calibrate the sensor with temperature.
I am using a 0-5VDC ADC and therefore need to amplify this signal to fully utilise my ADC range.
My intention is to use a wheatstone bridge (all resistors = 1k5 and the sensor resistor as listed above) connected to a single 5 V supply (see attached schematic).
In this configuration the common mode voltage varies between 1.7V and 2.5 V. The differential voltage is ≈0-1.45 V.
My intention is to use an INA326 with a gain of ≈3 to obtain a 0 -4.3 VDC range at the input of te ADC. (R1 = 56 k and R2 = 82 K)
QUESTION 1 : Is this the correct circuit to use as the datasheet has many options and I would greatly appreicate someones input on this ?
QUESTION 2: For my application, is it necessary to level shift the output as done in Fig 6 and Fig 7 of the DS ?
QUESTION 3: For my application is it necessary to use a output series resistor of 100 ohms ?
Thanks in advance.
Bob