Other Parts Discussed in Thread: LMP8601, LF356
Hi all,
I am trying to design a bidirectional constant current source. I have designed an improved howland current pump using LF356n. The op-amp is powered with +15V and -15V. The design is as shown in the figure. The load resistance is 5K and I have connected two LEDs in anti-parallel direction to visually display the change in current direction.
I want to achieve a load current of -2.5 mA to 2.5 mA. I am using LMP8601 to monitor the current.
The issue that I am facing is the voltage measured at Va is with a offset and the resultant load current is not completely bi-directional. I have connected pin no.1 and pin no.5 of LF356 to the ground and also I connected them using 20K pot as shown in its datasheet.
What have I missed in the design? How can I nullify the effect of offset? Should I use a different OPAMP?