Other Parts Discussed in Thread: THS4531, THS4120, THS4121, ADS8354, THS4531A, THS4521, OPA333
Hi,
I am trying to design a DAQ circuit with an op-amp leading up to an ADC. In looking at datasheets for op-amps, I wondered about the internal resistance for the op-amp to make sure that no (negligible) current is going into the amplifier and also because I have a source impedance between 1k and 5k for the sensor, so I don't want that to have an adverse effect on the voltage inputs to the amplifier. One op-amp I was looking at was the THS4531 (http://www.ti.com/product/ths4531). On the datasheet on page 11 under Electrical Characteristics, it says that the input impedance is 200kΩ, but that seems awfully low to me. I would expect something at least in the MΩ range if not higher. Typically, the resistance is high enough that it can be assumed no current passes into the op-amp. Can anyone tell me exactly what the datasheet is talking about when it refers to input impedance?
Thanks!
Matt