This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recommended Current Sense Device for Design

Other Parts Discussed in Thread: DRV110, AMC1100

Hello All!

I am working on a overload relay reference design using the DRV110 and was hoping I could get some input on what current sense / comparator device I should use. This design is for a line voltage of 120V (posted in photo). I looked at the portfolio for both products, but wanted suggestions since there are so many to choose from. 

I'd appreciate any and all help!

Thank You,

Ramon

  • Hi Ramon,

    I will get back to you on this.
  • Ramon,
    Is this 120V AC or DC?
    Most of our current shunt monitors go up to 80V common mode or less so 120V would require an AMC1100 type device or a magnetic current sensor. Let me know and I can see what we have that may work for you.
  • Hi Jason,
    Sorry to interrupt… My name is Idan and I'm electronic engineer for IAI Company.
    According to AMC1100 datasheet, the amplifier has Common-mode operating range of -0.16 to VDD1 (6V). In that case, why did you recommend it for current measurement above 120V? In my application I have to measure about 0-4A in voltage phase of 350V (High side or Low side). Can I do that using the AMC1100 amplifier? If not, do you have any recommendation for isolated amplifier that certified to high voltage standards?
    Thank a lot,
    Idan
  • Hi Idan,

    As I mentioned on your other post - The AMC1100 is rated to withstand 4250 Vpeak with a continuous working voltage of 1200 V, so there is no issue in using it for your application of 350 VDC.  You can do either high side or low side sensing - if you want to do high side, you'll need to create a floating supply in order to stay within the input common mode voltage range of the AMC1100. 

  • This would be 120V  AC.

    I am going to review the AMC1100 and see if it will perform well for what we are trying to do! Will get back to you!