This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High-speed amplifier selection

Other Parts Discussed in Thread: THS4541, THS3217, THS3215

Hello,

We want to choose two high-speed amplifiers, one for ADC board(four channel input)  and the other for DAC board(four channel output).

(1)  input signals of ADC boad are single-ended,  the frequency of  input signals is 0~100MHz,  amplitude of input signals is -2.0V~+2.0V, the gain varies within the range between -0.2dB and +0.2dB; 

input for ADC chip is differential, input common-mode voltage of ADC chip is around 1.0V, analog input span is around 1.6Vpp.

(2)  output signal of DAC board is single-ended, the frequency of output signal is 0~100MHz, amplitude of output signals is -2.0V~+2.0V, the gain varies within the range between -0.2dB and +0.2dB.

what amplifiers from TI can meet the requirement? 

Thank you!