Other Parts Discussed in Thread: OPA857EVM, OPA857
I received OPA857EVM and the mounted components slightly differ from the configuration mentioned in the manual.
The following resistors are not installed: R4, R16, R13, R14, and R9, R10 I believe are missing also.
I would like to know if that is standard shipping configuration.
Since the evaluation board I ordered produces no output in test configuration, I wonder if I have a faulty product that was not fully assembled or tested. I understand that the board should work without those resistors in place.