This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM102, LM101A Replacements?

Hi,

I'm currently attempting to simulate the "capacitance multiplier" below. I've come to understand that the op amps in the circuit, the LM102 and LM101A, are most likely obsolete. However, since I want to simulate a known circuit (not sure if incorrect simulations are due to choice of parts or not), I want to be able to simulate the circuit using LM102 and LM101A. Therefore, I was wondering if anyone had SPICE models for these two parts, or if anyone could suggest very close replacements for these two op amps.

Regards,

Michael Wu