Hey guys,
i need the right FDA for driving the ADS5482. Its just a one channel system, i don`t need any gain adjustments or other features just a simple single ended to differential amplifier which gives the best possible result referred to system accuracy and driving the ADC. It shall be used for capturing a higher voltage 2MHz Signal which has some less powerfull harmonics up to 50Mhz. The signal can be easily conditioned to the right amplitude to fit the requirements of the ADCs input range, i will use a low order Bessel AAF to be sure that there are no high frequency signals above the nyquist frequency..
Any recommendations?
Greetings from austria!