Other Parts Discussed in Thread: BUF634, BUF602
Hello,
I need to produce a 3.3Vpp [0 to 3.3V] square wave/clock signal at 60MHz and I plan to use the MXO45HSTLV-3C-60M0000-ND oscillator:
1) I need to know whether this oscillator will allow me to generate clean square-waves at 60MHz.
2) I have never really worked with this type of oscillator before so could someone provide me with a circuit which shows how to connect and apply this device?A circuit which will allow me to generate square waves to my specifications?
3) I need the generated square waves to drive a 50ohm load so will require approximately 65mA of output current. For this I plan to feed the generated square wave from the oscillator through a high speed, high current buffer such as the BUF634. Will this two stage set-up work?
BUF634: