Other Parts Discussed in Thread: PGA309
I have a pressure measurement system based on the PGA309 amplifier. Currently the PGA is calibrated/programmed via I2C. I need a One Wire interface/programmer to perform the same operations (calibration, EEPROM programing via PGA, etc.)...So far the only option I found is a USB DAQ platform which is part of the evaluation module. Is there anything else available? Can I purchase the USB DAQ board alone? I only need to use the One Wire interface.
Thank you