Hi, I am using a TLV2460 OpAmp as a voltage follower. 99% of the time (99% DC) there is a 2.65V difference in the non-inverting input and the output of the OpAmp. The non-inverting input sees 2.65V, while the output is at GND. The inverting input is connected to the output (voltage follower). My question is that since the output is connected to ground, and the IC is only rated for p/m 80mA, will this exceed the maximum ratings since it is trying to source 2.65V directly to GND?
I have measured the current of entire circuit and doesn't go over 25mA which leads me to believe it is the proper range.
Thank you.