Other Parts Discussed in Thread: INA199
Hi Team
Please check my understanding regarding INA199’s output swing vs output current.
This device cannot be used with 5V supply and low output resistance like 1khom because output current can be ~several mA resulting in very narrow output voltage swing. Is that correct? How much input impedance at output of INA199 should be? From the fig. 6 and fig.7, I think the output current have to be limited less than 1mA if 5V supply is use.
Thanks,
Takuma Ito