This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA204 PIN Connection



Hello ,

How should I connect the PIN1/PIN6/PIN7/PIN9 , if I don't need adjust the offset volatge of amplifier ?

From the following diagram , if we need to leave  it floating?


It seems the part is very old and its datasheet is not as well as the style TI used now .

Thanks.

  • Hello Kevin,

    Yes, you can leave those pins floating if you don't need to adjust the input stage offset.

    Pin 6 and Pin 7 are the optional input offset trim pins. Pin 1 and Pin 9 are actually sense points for the output voltage of the input stage amplifiers: VO1 is the output of input amplifier A1, and VO2 is the output of input amplifier A2.

    Best regards,

    Ian Williams
    Linear Applications Engineer
    Precision Analog - Op Amps
  • Hello  Williams,


    Got you , thanks so much .


    Your response is very fast ,exellent!

    Regards

    Kevin