Other Parts Discussed in Thread: OPA454, LM324, LM324A
Hii
I want to design constant 10mA current source independent of load resistance(Load is varies from 10 ohm to 5k ohm). I have tried Howland current source circuit and i achieved 5.2mA constant current over 10-5k load with 12V input voltage and +/-15V supply voltage of op-amp.
I have attached the circuit with this. Here I got only 5.2mA constant current , in order to increase current capacity if I change the resistance value from 2.3K to 2k then current is not constant over 10-5k range.
So what should I change to get constant current of 10mA