Hi,
I'm simulating AMC1301 in Ti TINA. My simulation is based on the following file. However, I noticed the chip doesn't work if VDD is below 4.5 V. The datasheet mentioned it operates at 3.3 V or 5 V. So, which one is correct?
Thanks,

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.