Other Parts Discussed in Thread: INA122
Hi, we're currently working on a design using the INA122 and have a couple questions.
1) For the spec on the INA122 web page that says
|
Output Offset (+/-)(Max)(uV) |
100/G |
How should that be interpreted? 100uV of offset for every unit of gain (therefore if I set my gain at 500, I can expect up to 50mV of offset?) or 100uV divided by your gain (100uV / 500 = 0.2uV offset?)
2) We're also using a small Vref to offset the output of a loadcell. Mainly we are measuring compression (under compression the difference between S+ and S- are roughly 2mV) but also would like to measure a small range on tension (so the S+ and S- would be -0.1mV) which is why we want to use a small offset rather than tie Vref to GND.
It's working fine, but we are wondering what the Vout gain and offset accuracy is now? Can we still assume the 1% gain error as declared in the datasheet? And % Vout offset?
Thanks in advance
cynthia